This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A7100的控制问题

Other Parts Discussed in Thread: TPS7A7100

大家好:

TPS7A7100这款芯片使用6个引脚控制输出电压,请问我是否能用单片机的开漏输出模式连接这些引脚去控制输出电压?

如果可以的话,请问可以在上电之后改变引脚连接去改变电压?

如果不可以,能否推荐一款,几百毫安电流,1.2-3.3V输出,可以使用单片机IO/IIC或者其他方式控制输出电压的电源芯片芯片。LDO或者DCDC都可以

  • Hi
    可以的,如果你的电压变化刻度是0.05V每步, 可以通过6个I/O口控制,见datasheet第19页的电压输出配置。
    如果你的输出电压希望做更微小的调整,可以按照datasheet 第20页接反馈电阻的方式,单片机I/O PWM输出加RC滤波器成直流或者DAC输出,通过二极管以及一个电阻的方式连接到FB脚, 此时(单片机输出-0.7V)/R + (Vo-VFB)/R1= Vfb/R2。