This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4128是否可以作为恒流源使用

Other Parts Discussed in Thread: LM4128, LM334

想要设计的应用是PT1000温度检测,想使用LM4128作为恒流源用 ,将RL电阻替换为PT1000然后ADC采样(精度为10位ADC),温度误差为+-2度。想问一下LM4128,  Iout=2mA ,精度为0.5% 是否能达到这个要求?IGND电流如何计算? 恒流源芯片LM334是否能满足相同的要求??

  • Hi,

    你好!我觉得你的温度检测精度可以分成两部分考虑,一是电流源输出20mA电流的精度,另一个是ADC采样。
    我大概算了一下,你的应用里大概是77mV/C。电流源的部分,如果0.5%的精度,最终反映在热敏电阻上的电压也就是0.5%的误差,足够满足要求了。GND电流我觉得影响不大,你可以通过调整Rset使得输出电流是比较准确的20mA。
    ADC采样部分受ADC精度和分辨率限制。
  • Hi

        LM334也是可以的,这个是专门做电流源的芯片,但是只有10mAMAX的电流,如果要20mA要做电流扩展。