Other Parts Discussed in Thread: TPS92641
HI,
我正在用TPS92641控制大约500个0.5w白光灯发光,10个灯珠串联,并联50条,因为每个灯珠需要3V@120mA,总电流要达到5A。
输入电压电压48V;
Fsw=(330kk+20k)/(20k*33k*1200pf)=442kHz
Rcs=0.15
两个MOS管用的是PSMN069_100YS
我的PWM固定在200Hz,占空比调到100%,电感用的是100Uh,模拟电压调节范围在0-2.5v,
负载我无论并联多少灯,总电流最大值基本都在900mA左右,没办法在上升,我试着将Rcs换成0.1或者0.05都没有改变!
能给出什么建议吗?