This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010和TPS61230A使用疑问

Other Parts Discussed in Thread: LMR64010, BQ24040, TPS61230A, TPS61230AEVM-767, LMR64010XMFDEMO

产品为一个手持TPMS,电源原理图如下(图一),我们使用BQ24040给电池充电,使用TPS61230A将电池电压升压到5V,在通过LMR64010将5V升压到11.5V给Lin TJA1021供电(11.5V负载如如下所示图二和图三,此时视频 125K的12V为关断状态),当输入使用电池测试发现上电LMR64010将电压拉低到1.7V左右(此时TPS61230A输出也为1.7V左右),但我们将LMR64010前的0欧电阻断开后测试TPS61230A输出5V正常,,但我们将LMR64010与TJA1021之间的0欧电阻去电,LMR64010输出11.5V正常将电源输入改为使用DC Source(设定为3.8V,限流设定到4A)同样出现的现象(带TJA1021通电拉低到1.7V,不带输出11.5V正常),测试LMR64010的SW波形图如下(此时不带Lin,芯片输出11.5V正常),感觉SW波形不正常(图4)。

但是我们将LMR64010的输入端直接改到3.8V供电(与TPS61230A的输入为同一处,此时3.8V使用的为DC Source),直接带TJA1021,LMR64010输出11.5V正常(觉得很奇怪)。

当改为LMR64010使用3.8V供电,通过软件让FSK芯片 ATA5781工作,使用5V供电(R83焊接,R82未焊接),一旦提供PWM让震荡电路工作,TPS61230A和LMR64010瞬时就无输出,需要重启输出才能恢复正常,恢复正常后再次打开震荡电路,再次两个无输出。哪位大侠能帮忙分析下两个现象吗?

1、为什么使用TPS61230A升到到5V,LMR64010将5V升压到11.5V这种方式不能给TJA1021供电(Lin工作电流在12V/50mA左右)?此时LMR64010的波形正确吗?

2、为什么FSK芯片 ATA5781工作起来,TPS61230A和LMR64010瞬时就无输出?