用UCC27611搭建的驱动GaN FET电路,在FET的Drain极不加电源时,UCC27611输出波形正常,NGA的Drain极加电时,UCC27611输出端检测到干扰波,请帮忙看下是什么问题,谢谢
电路图如下:
不加80V偏置电压,测得EPC2016C的GS间的电压波形:
加了高压偏置电压,测得GS间的波形:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
建议贴出来实验波形,GS 电压一般是受DS电压影响产生的干扰信号,在DS dv/dt 变压大时一般是正常现象,谢谢。
驱动端口离MOSFET距离5mm,中间串有两个0201的0欧姆电阻。