Other Parts Discussed in Thread: TPS61165
Hi,
我想请教一下关于TPS61165芯片的几个问题:
1. TPS61165的反馈电压TPY值为200mV,驱动电流是通过Rset的大小决定的,比如Rset为1Ω,LED电流就为200mV/1Ω=200mA,那如果Rset值发生变化时,LED电流也相应变化,那输出电压会有相应变化吗,怎么变化?(查看手册说,输出电压是Vin~38V之间,大小由LED的数量*LED的压降决定的,那输出电压就是不变的咯,我感觉不是这样的)
2. 我目前选择的LCD屏手册中提到背光输入电压是8.7V~10.5V(当LED的电流为210mA),而我设计的TPS61165的输入电压为15V或者11.1V,根据TPS61165手册中提到输出电压是Vin~38V,那明显就会对我的LCD屏背光电路造成损毁,请问在设计中有什么可以改进的吗?如下为我的设计原理图。