This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ25071-Q1应用问题讨论

1、 BQ25071-Q1器件是不是线性的,加入输入5V,输出3.5V,那么中间1.5V的压降是不是器件自己的功率耗散?
2、EN管教虽然拉低使能,但拉高只是限制了充电电流,由于我们的电池同时连接在充电和负载上,在电池供能的时候是不是必须将充电芯片完全关闭?

     好像只能将IN的电压断开,是不是这样?没有充电截止电流?充电截止条件?

3、没有找到开始充电的阈值电压,就是电池电压低于多少就会进行充电?检测至电压低于多少V会再次充电?
4、TS使用LDO的输出进行分压,那么IN是不是必须高于5V,否则LDO电压将降低,会影响TS的判断,这个问题结合1一起考虑

  • Hi
    1. 和LDO一样,芯片的功耗就是输入电压减去输出电压,乘以充电电流。
    2. 没有输入,电池会给系统供电。
    3. Once the BAT output reaches the overcharge voltage threshold, CHG goes high impedance to signal the battery is fully charged. When the battery voltage drops below the recharge voltage threshold the CHG output is pulled low to signal the host of a new charge cycle.
    Battery overcharge voltage threshold , 见参数表。
    4. 是的,LDO输出4.9V,建议输入大于5.1V, 才能正常输出,否则LDO输入会偏低。