This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL594CDR的并联逆变器

第一次TI发帖,有什么描述不对的请各位大牛指正。
最近在做一款并联逆变器,DC220V-AV220V,输入范围是DC180-275V,  5个模块并联,SPWM是用一个监控模块的,DCDC是用TL594CDR做的全桥电路。现在存在一个问题,当低压时出现不均流情况,测试发现TL594CDR占空比都达到最大,但是最大占空比不一样(有的44%,有的46%),导致母线电压不一样。之后对同一批次的芯片装上同一块板,发现确实存在最大占空比不一样的情况。
请问一下几个问题:
1,TL594CDR出现这种情况属于正常范围内吗?有没有其他精度更好的芯片可以替换的?
2,能从芯片外围的参数改善这种情况吗?