This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS63070电压输入范围问题

Other Parts Discussed in Thread: TPS63070, TPS61200, TPS63060

如题,据手册上显示该升降压芯片的电压输入范围是2V-16V输入,我是打算按2.5V-5.5V输入,5.5V输出设计的,但是在无负载情况下,实测电压在2.73V以下的时候,TPS63070输出只有0.22V左右。

请问是什么原因导致它2.5V无法启动,是DATASHEET描述有误?还有什么升压芯片,能满足我这样的输入要求,然后开关电流不会太大,器件体积及外围电路较小的,因为我前级打算加高低压保护,我用的LTC4365会限制我之前用的TPS61200的带载能力,导致加负载低于4.3V以下就输出异常了,tps63070不会它也不需要保护,但是它低于2.73V就自动没输出了,很尴尬!