This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

充电芯片BQ24765,充电无电流

Other Parts Discussed in Thread: BQ24765

我们主板上的充电芯片是BQ24765,调试电路时遇到,开始给电路充电时,输出电流是OK 的,但过了1,2分钟后,输出电流为0,拔下适配器后,必须等上近1分钟,再插上适配器,才有输出电流,而且反复的给电池(电池最大电压是16.8V)充电,电池也能充进电;其中无论是否有电流:DCINA 为18V> 4.5V, and VDDSMB 为3.3V>2.5V,ACIN为2.6V > 2.4 V,CE=3.1V为高电平,VDDP为6V,VREF 为3.3V;而且测得bq24765 switching frequency是:当电感Lout=15uH时,Fs = 50KHz,当电感Lout=3.3uH时,Fs = 79KHz。请帮忙解决,谢谢!