This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TIDA-01573激光二极管驱动器使用的一些问题

Other Parts Discussed in Thread: LM5000

     我近期按照官网上的PCB文件和BOM,自己做了几块激光二极管驱动板,激光管使用 OSRAM  SPL_PL90_3,实际测试过程中遇到如下问题:

    1. 原理图中R5,R6,R7,R8 等4个并联电阻的作用是什么?将激光管与这4个电阻并联使用,激光管可发光,去掉这4个电阻后也可发光,是为了和D1二极管构成续流吗?

   2. 从初步测试看,激光管发光的光强不太稳定,适当减少储能电容C2,C3,C6,C7,C8,C9容值,发光强度依旧不太稳定,请问一下可能是哪个方面的问题?

     高压电源使用的35V,0.2A的LM5000方案,从示波器上看发光过程中电源无明显恶化。

     XLMG1020输出端脉冲基本正常;不接激光管时,XLMG1020输出端(EPC2019 门级)脉冲信号质量较好,接激光管时,XLMG1020输出端(EPC2019 门级)脉冲信号存在一定震荡,震荡电平可能会超出EPC2019导通的判决阈值。貌似激光管激发过程中能量通过EPC2019对  XLMG1020输出端有影响。

    XLMG1020输出端脉冲宽度尝试过10ns和20ns,上述问题均存在。