tps61087 空载反馈电压0.3v,输出明显不对了,电路图按照数据表里的,电感3.3uh,R1和R2分别为18K,200K,不知道哪出问题了,谁有做过这款产品的请帮忙回答一下,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tps61087 空载反馈电压0.3v,输出明显不对了,电路图按照数据表里的,电感3.3uh,R1和R2分别为18K,200K,不知道哪出问题了,谁有做过这款产品的请帮忙回答一下,谢谢。
你好,
输入电压5V,按理说也不应该啊,我把散热片接地了会不会影响,谢谢
你好;
我用万用表量了一下SW脚是5V,输入5V,通过电感到SW,然后到二极管输出4.8V,芯片就没有输出,然后我焊接的时候用的热风枪,芯片有没有烧坏的可能,谢谢。