This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高输出电压,大电流输出DC-DC设计!

Other Parts Discussed in Thread: LM25088, TPS40060, LM3150

 我须要设计一个DC-DC降压电路,具体要求如下:

1. 输入电压:24V-42V

 2. 输出电压可调(准备用MCU控制反馈电阻的方法实现调压),最高为20V,不考虑数字IC。

 3. 输出电流最大可做到4.5A

 我现在是须要确定TPS40060或LM25088两个芯片能不能达到我的设计要求,哪一个会更合适呢?

 因为是电池供电,效率至少在85以上? 满载(90W)时5分钟内不能烫手!!

还有就是价格,我希望成本不要太高,芯片在10RMB左右的,如有可满足我须求的芯片请推荐,谢谢!