你好!
TPS2549设置在CDP模式下,
连接华为荣耀10时,充电电流可以到达1.42A,连接IPHONE 8 Plus时充电电流为1.46A;
但是连接华为P20时,充电电流为0.46A,连接小米MIX2时,充电电流0.46A
请问是因为TPS2549的不支持P20,MIX2,还是因为手机端的原因,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
TPS2549设置在CDP模式下,
连接华为荣耀10时,充电电流可以到达1.42A,连接IPHONE 8 Plus时充电电流为1.46A;
但是连接华为P20时,充电电流为0.46A,连接小米MIX2时,充电电流0.46A
请问是因为TPS2549的不支持P20,MIX2,还是因为手机端的原因,谢谢!
建议您确认一下P20,小米mix是否支持CDP-auto
The TPS2549 device also integrates CDP mode, defined in the BC1.2 specification, to enable up to 1.5-A fast
charging of most of portable devices, meanwhile supporting data communication. In addition, the device
integrates the DCP-auto feature to enable fast-charging of most portable devices including pads, tablets, and
smart phones.