最大电流13A,前面用两单支管子发热很严重,后改用四只管子并联均流,现在的问题是
- 如果四管并联,输出电流在0~0.9A时可以正常工作;电流超出就会烧毁Q1管。
- 两只管子可以正常工作,但是发热比较严重。输入电压是直流恒压24V。
手册中CSD18531Q5A的耐压是60V,持续电流19A,手册SOA也可以通过,电路中PWM频率是50KHz,请问大伽们,这有可能是什么原因造成的呢?
MOS管的Layout如下图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最大电流13A,前面用两单支管子发热很严重,后改用四只管子并联均流,现在的问题是
手册中CSD18531Q5A的耐压是60V,持续电流19A,手册SOA也可以通过,电路中PWM频率是50KHz,请问大伽们,这有可能是什么原因造成的呢?
MOS管的Layout如下图:
你好,请问CSD18531Q5A这款MOS和UCD7138驱动器合适一起使用吗?我看了这两个数据手册,不知道有什么合不合适的情况,麻烦指导一下