This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030输出电压不稳定

Other Parts Discussed in Thread: LMR14030

LMR14030输出不稳定,求大侠支招。

使用LMR14030,输入电压12V  1A电源适配器,输出电压3.8V,试产主板,有部分主板输出异常,有部分主板相对更稳定一些。输出异常的具体表现为:上电初期,输出电压正常为3.8V,测试一段时间(几分钟,几小时不等)后。输出电压出现抖动(输出电压变低,由3.8V 开始下降,不规则的下降到3.3,2.7,直到0V),功率电感前端(SW管脚)波形不规则(开关波形紊乱)。 不管是空载还是使用电子负载带载测试。都会出现相同的现象。

1、尝试将新的LMR14030芯片换到易出问题的主板上,问题依然存在(排除单体芯片的问题)。

2、出现输出不稳定问题的主板,有时复测,输出是正常的(怀疑芯片并未损坏),但测试一段时间后,输出会抖动,最后变为零。

3、外围器件规格:输入电容,4.7uF*6,+10nF一颗+100nF一颗;使能端采用470K和100K通过VIN(12V)分压产生;RT/SYNC外部电阻49.9K;SS外部电容22nF;SW功率电感4.7uH(饱和电流6A),肖特基二极管(正向电流2A,反向耐压30V),输出电容47uF*6+100nF一颗+2.2uF一颗;反馈电阻 100K和24K(其中100K并联了一颗33pF电容)。