This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072充电电流太小

最近接手一个项目,其中充电部分电路图如下:

在实际使用过程中,通过测试发现,在恒流充电阶段,充电电流只有不到8mA。将TD脚接一个高电平,充电电流差不多就有50mA.这确实让人费解。

电源输入是PC的usb口的电源。另外,测试过电池,恒流充电时,充电电流可以达到210mA.请高手么给个意见。

  • TD引脚的电平并没有影响恒流充电电流的大小,只是没有充电截止这一过程:

    ConnectTDto a logic highto disablechargetermination. Whentermination is disabled,the devicegoesthrough the pre-charge, fast-charge andCVphases,then remains in the CVphase.

    ILIM,及ISET的配置与图中的参数是一样的吗??

  • TD脚按理是不该影响充电电流的,为什么会有影响了?难道测到的只是一个假象?

    是的,参数是原理图一样的。不然,贴这个电路图就没有多大意义了。关于ISET脚的电阻,我看规格书“the voltage at ISET reflects the actual charging current and can be used to monitor charge current.”,这一句说的意思是检测充电电流用的,电阻随便设置就可以了,只要在描述的规格内。1k是满足590 Ω to 3 kΩ的了。

    ILIM接的电阻,按公式算的最大大流的电阻。