This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS23753转12V输出48V电压不稳的问题,请求解答。

Other Parts Discussed in Thread: TPS23753, PMP8803

工程师,您好!

我借鉴原来的一个用TPS23753转5V输出的电路,想改成12V输出,原电路如下图,参考电路如图2或链接(即开发板:PMP8803)

www .ti.com.cn/cn/lit/df/slvrb28/slvrb28.pdf

但是实际应用中,我们按照参考电路变更了物料后,发现12V输出不稳定,类似锯齿波高电平12V低电平8.8V左右,最好测试发现是48V输入不稳定,实际输入电压52V,但是输入波形类似方波,正占空比只有35%。请帮忙 分析一下原因。

做过几个测试:

确认过DEN管脚的电阻阻值24.9K无误;

CLS管脚的电阻我们更换为1.24K或90Ω现象并无变化。