要求:输入5~24V,输出5V 2A
使用了好多芯片,问题出现在低压输入时,例如输入5V,但输出5V不稳定或根本输出不了5V(例如TPS54240,仅输出了2.3V,或输出一直在高低高低变化);
求推荐,可用的芯片,输入低压时(5~6V),输出能稳定在5V;
谢谢~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要求:输入5~24V,输出5V 2A
使用了好多芯片,问题出现在低压输入时,例如输入5V,但输出5V不稳定或根本输出不了5V(例如TPS54240,仅输出了2.3V,或输出一直在高低高低变化);
求推荐,可用的芯片,输入低压时(5~6V),输出能稳定在5V;
谢谢~~
你试过? 我查阅了TI所有的相关参考设计,压差没有低于5V的。TPS54240手册中写着VIN>BOOT+2.1V 我测试时确实发现,提高输入,将输入输出压差大于2V立马好使,低于这个值,输出不行。