能否帮忙推荐一个12V输入,3.3V输出,电流在120A的方案?
TPS53641可以吗?我看手册上Vo max=2.5V,但我看过国外一个设计上就是用来输出3.3V的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS53641可以吗? 网站介绍的最大2.5V是最大输出吗?
TPS53679的电流有点大了。