This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

适用于激光雷达的纳秒级激光驱动器参考设计 TIDA-01573



先接通  J1加了5.5V限流0.1A的电压

然后接通 信号发生器 100kHz  3V  100ns

最后接通的J2  电压10V限流 0.2A

但是在接通J2时候,发现J2的电压一直上不去(约为1V多),此时电流一直是0.2A