This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

禁止BQ24780S内部REGN LDO输出降低功耗问题



问题一:REGN LDO的工作条件:6-V linear regulator output supplied from VCC. The LDO is active when ACDET above 0.6 V, VCC above UVLO. Connect a ≥ 2.2-µF 0603 ceramic capacitor from REGN to GND. The diode between REGN and BTST is integrated.简而言之就是VCC电源在工作范围内,ACDET引脚工作大于0.6V

现在测试发现不联接SMBUS的两根线对其配置,BQ24780的VCC电源消耗电流是15uA左右,但是一旦联接SMBUS对其通讯,不管是充电允许还是不允许只要通讯配置,REGN引脚输出6V,BQ24780的VCC电源消耗电流是400uA左右。即使是给ACDET接地,LDO输出任然为6V。请问这个问题怎么设置不允许LDO输出?

问题二:数据手册“8.2.2.3 Reduce Battery Quiescent Current”章节中设置ChargeOption0() bit[1] to 1意义是什么?因为实际这个位是Reserved的?