This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ40Z50 R2 Full Charge Capacity更新容量过低问题

Other Parts Discussed in Thread: BQ40Z50-R2, BQSTUDIO

BQ40Z50-R2在bqStudio软件中读取 Full Charge Capacity容量时,发现都达不到满充时的容量值,大约只有设计容量的85%左右。

设计为两串3并的一个电池组,其它都正常。相关参数

Cell 1 chg voltage at EoC  4200mV

Cell 2 chg voltage at EoC  4200mV

Cell 3 chg voltage at EoC  0mV

Cell 4 chg voltage at EoC  0mV

current at EoC   50mA

Qmax Pack  更新容量大于设计容量

请问对Full Charge Capacity有影响的有那些设定值?