This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78412应用问题,求熟悉此芯片的高人答疑

Other Parts Discussed in Thread: BQ78412

我应用bq78412是在两节串联的12V电池中的,两个BQ78412都隔离并与整个板子的系统也隔离,两个通讯接口也都隔离。

采集电流的RS+和RS-都接在串接电池的连接线上(1mohm内),第一个78412以第一个电池的负极(串起来后24V的总负)为地,第二个78412以第二个电池的负极为地

问题:每次把线接好后,就发现测第一节电池的78412已经坏了(自己产生的3.3V输出只有1.448V),重新单独上电(直接第一节的连接线,不接第二节)也不会再改变。已经这样坏了5,6个片子了,尝试各种方法,百思不得其解,请高手指点~

备注:板子没有焊接问题,也没有接错元件等错误,就是不知道这样子对串联电池的接法会不会有问题~