This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5017上电瞬间 二脚位置烧坏

Other Parts Discussed in Thread: LM5017

做过输出短路测试LM5017启动短路保护,这个短路测试是LM5017运行前和运行中短路都测试过,LM5017都没问题,现在上电LM5017的二脚位置直接烧坏,LM5017输入端串联了一个2A的防反二极管没有串联电阻,,使用的电池50V上电,测试百次插拔上电示波器抓到的最大的波形都是58V的,5017启动电压14V输出10V,关闭电压11V,输出的10V是给MOS驱动使用,建立10V电压需要100mS,开启MOS是在上电后1S时间,实在是想不到说明原因导致的,哪位大神也遇到这个问题