Other Parts Discussed in Thread: BQ24133
BQ24133的单节锂电池充电,配置充电电流为2A,输入电压为USB 5V,当电池放电进入过放保护之后,必须要使
用输入能力大于5V2A的适配器充电到3.5V之后,才能使用5V1A的适配器进行充电。
1、为什么电池进入过放保护之后,BQ24133开始充电时没有进入涓流充电(预充电,配置充电电流的10%,200mA)
,而是直接进入了恒流充电。BQ24133进入涓流充电的条件是什么?
2、怎么样设计可以让BQ24133配置的充电电流为2A时就算使用5V1A的适配器也能正常充电。
在使用5V1A适配器充电时,OVPSET并没有低于0.5V,并且PVCC端和AVCC端都没有压降。使用datasheet上标准参考设计(
Figure 1. Typical Application Schematic (12V input, 2 cell battery 8.4V, 2A charge current, 0.2A
pre-charge/termination current, 2A DPM current, 18V input OVP, 0 – 45°C TS)
)。