外部输入24V,输出5V,外加50欧姆负载电阻。当去掉负载后,电路输出周期性有无。
当吧限流电阻去掉,短路后,出现在177度后半小时突然出现供电电流持续增加,然后输出变成0,这个时候电源电压也变成0,
到了常温我把D2,Q1(考虑他们与输入电流变大直接有关),换掉,个了一段时间常温下又好了
在该电路中考虑到成本,R1,Q1,D2是175度的,C8是175度10V,D1是175度24V(抱歉我图上标记不对)
C1,C2是35V的VISHAY 150度电容,其他电阻是155度,电容是150度50V的
在实物图中100毫欧姆是有的,TVS被我卸掉了