Other Parts Discussed in Thread: UCD3138, UCC27211
前辈们好,
我仿照UCD3138的全桥硬开关开发板做了一个全桥电路。
由于我使用的初级MOS管驱动器不是UCC27211,导致驱动PWM信号延迟200ns,我测试了UCC27211的延迟约30ns,从而电路PWM驱动时序发生变化。
初级MOS管和次级同步整流管驱动如上图,紫色和绿色是初级驱动,黄色和蓝色是次级驱动,可以看出,由于初级驱动PWM信号经过驱动器IR2110后发生了200ns的延迟,从而使初级和次级驱动信号之间出现了重叠。
我尝试着增大初级驱动和次级驱动之间的死区达300ns,使重叠区域消失,也就是缩短同步整流驱动信号的导通时间。可是电路又会出现振荡,如下图:
我不知道为什么会出现振荡,此时,输入电流会增加0.6A。我观察的现象是:通过增加初级和次级PWM的死区,虽然使的两者因初级延迟而产生的重叠消失了,但是初级和次级驱动的占空比也相应下降。我想不通,主电路为什么会产生振荡?还是什么方法可以消除由于驱动器IR2110带来的200ns的延迟的不利影响吗?