This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO 选型:最大输入电压8V, 输出 3.8V ,1A, 静态电流5uA? 找到TPS7A26, 这个只有0.5A,能否用两颗合并使用。合并使用会有什么问题嘛?

Other Parts Discussed in Thread: TPS82150, TPS82140

 

具有电源状态良好指示的 500mA 18V 超低 IQ 低压降 (LDO) 线性稳压器,

超低 IQ:2.5µA
输入电压:2.4V 至 18V
可用输出电压选项:固定:1.25V 至 5V
可调节:1.24V 至 17.45V
工作温度范围内的精度为 1%
低压降:500mA 时为 550mV(最大值)
漏极开路电源状态良好指示输出
内部软启动限制浪涌电流
热关断保护和过流保护
运行结温范围:–40°C 至 +125°C
与 1µF 输出电容器一起工作时保持稳定
封装:WSON-6