Other Parts Discussed in Thread: LM3414
请问,LM3414用PWM调光为什么效率很低,输入28V,1.5A,输出端串联了8个灯,输出电压为24v左右, 通过调Riagd 电阻,电流在350mA到1A驱动效率能达95%,当设置LM3414固定输出为1A,然后用PWM调光,电流从350mA到1A,效率从65%到80%变化,请问为什么效率低了这么多,而且随占空比的增大而改变。
频率500Khz,电感47UH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM3414
请问,LM3414用PWM调光为什么效率很低,输入28V,1.5A,输出端串联了8个灯,输出电压为24v左右, 通过调Riagd 电阻,电流在350mA到1A驱动效率能达95%,当设置LM3414固定输出为1A,然后用PWM调光,电流从350mA到1A,效率从65%到80%变化,请问为什么效率低了这么多,而且随占空比的增大而改变。
频率500Khz,电感47UH
PWM为100%的时候也低,大概效率只有80%,这种情况正常吗?可能是哪种原因造成的?
在不加pwm信号的情况下,效率大概有93%
发现如果加PWM信号,占空比在50%以下效率偏低,在70%以下,占空比在50%以上,效率在80%以上,请问这个效率为什么在占空比50%
一下效率偏低,从硬件的角度来说这个效率和占空比有没有关系?若是有,存在什么样的关系,谢谢
调光状态下的效率不能只运用万用表测试电流电压来计算,应该计算导通时间的电流和电压,那个电流和电压需要用到示波器和电流探棒,那个值和你的满载工作效率相差不大。