我们在使用LM5066有如下的疑问,请帮忙解答下,谢谢!
(1)所有寄存器的每一个标志位为1时,代表有效?
(2)MFR_SPECIFIC_17:READ_DIAGNOSTIC_WORD(E1h)的BIT14 IIN_OP_WARN是表示电流还是功率的警告标志位?
(3)通过I2C给lm5066的MFR_SPECIFIC_03:MFR_IN_OC_WARN_LIMIT(E1h)写入0.3V的电流,通过电子负载给MOSFET的后级电路负载0.4V的电压,即触发输入电压过流警告。为何可在0x78,0x7C,0xE1读到VIN_UV_fault
(4) dv/dt输出控制电路,只有在使用dv/dt启动时才需要,但是去掉这一部分电路后,OUT为0,MOSFET没有工作;
(5) dv/dt输出控制电路连接上,TIMER引脚测量到的时间是否包括这一部分的时间,若包括,如何确定TIMER的时间?