This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24170 充电电压 达不到12.6V,求指导!



TI的工程师你好:

我用的是BQ24170做为充电IC, 适配器采用数字电源,输出电压15V,设定ACSET是5A;BQ24170充电电流3.75A,CELL选择经过2k电阻接到VREF 3.3V。

现在出现了以下问题:

1、我将12.6V锂电池(说明书上,标称11.3V,三节4.2V串联)放电至10V,开始充电,只能充到11.3V就停止充电了,STAT灯由常亮变成闪亮,观测SW的PWM由连续变成断续。

不是应该充到12.6V充电电流才变小吗?为什么到11.3V就停了?