This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B开发问题

Other Parts Discussed in Thread: BQ51013B

最近开发一个项目用到BQ51013B这颗芯片,阅读数据手册以及开发板资料后有2个问题需要请教:
1、FOD引脚
   在开发板资料sluua44a.pdf的第3页 Figure 1. HPA764 Schematic中,FOD引脚通过R17=20K接RECT引脚,通过R2=150R接地;又根据数据手册bq51013b.pdf第32页 8.2.1.2.5 Current Limit and FOD中的描述可以知道Ros(R17)和Rfod(R2)是由FOD校准来决定,其中又说道需要用一个软件Foreign Object Detection (FOD) Calibration/Tuning Tool来完成。我是否可以这样理解:通过调整Ros(20K)和Rfod的值进行整流功率检测,使得整流输出RECT引脚的电压通过FOD引脚反馈到发射端,控制发射功率从而使RECT引脚在一个合适的电压值?如果是的话,这个值是多少呢?

2、ILIM引脚
   在开发板资料sluua44a.pdf的第3页 Figure 1. HPA764 Schematic中,ILIM引脚通过R4=110R的电阻到FOD引脚,再通过R2=150R的电阻到地;又根据数据手册bq51013b.pdf第16页 7.3.4 RILIM Calculations中的描述可以知道
Ilim=Klim/(R1+Rfod)=314/(R1+Rfod)   限制保护电流
Imax=Kmax/(R1+Rfod)=262/(R1+Rfod)   输出最大电流
Ilim=1.2xImax
所以当R1+Rfod=110+150=260R时,Imax=1A(输出最大电流),Ilim=1.2A(限制保护电流),这个计算方式对吗?