Other Parts Discussed in Thread: TPS7A49
Hi Team:
在使用TPS7A49过程中有一个问题,前级输入为13V,输出要12V(系统输入为DC5V,使用升压芯片直接升压到12V因有噪声等问题,所以选择加一颗LDO,使前端升压到13V后再降压)。目前测试发现,起初输出一切正常,但用手触碰到芯片后输出会增大到14V,或者降压到0V,同时测试发现出Pin 6脚NR/SS与正常时不一样,异常芯片时为7V左右,正常时测试再1.6v左右。这种现象断电重新上电后恢复正常。如下是电路原理图,请帮忙看下是否有问题,哪方面原因会引起这种情况。