This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教GPC回复报告化学ID问题

Other Parts Discussed in Thread: BQ27426

上传GPC数据后官网回复报告如下:

Chemistry ID selection tool, rev=2.47

Configuration used in present fit:
ProcessingType=2
NumCellSeries=4
ElapsedTimeColumn=0
VoltageColumn=2
CurrentColumn=3
TemperatureColumn=1

Best chemical ID : 2487 Best chemical ID max. deviation, % : 1.08



Summary of all IDs with max. DOD deviation below 3%

Chem ID max DOD error, % Max R deviation, ratio
2487 1.08 0.54
1976 1.27 0.35
2407 1.29 0.91
245 1.37 0.52
1982 1.39 0.53
2286 1.39 0.27
231 1.44 0.62
221 1.46 0.74
218 1.46 0.69
2102 1.47 0.27
1301 1.48 1.15
1741 1.48 0.51
1323 1.53 0.28
1331 1.53 0.7
1340 1.54 1.12
2442 1.57 0.35
2405 1.57 0.8
261 1.58 0.55
1991 1.61 0.4
1954 1.64 0.45
227 1.64 0.47
2127 1.71 0.24
1325 1.73 0.36
253 1.76 0.39
297 1.77 1.16
2047 1.77 0.29
206 1.77 1.56
2053 1.78 0.75
234 1.79 0.8
239 1.8 0.32
252 1.84 1.11
2078 1.86 1.44
2151 1.87 0.24
1332 1.89 0.81
1352 1.89 1.21
3596 1.9 0.75
1314 1.9 0.43
2048 1.91 0.35
2188 1.95 0.45
2309 1.95 1.49
2135 1.96 0.46
212 1.97 1.97
2126 1.98 0.86
1996 2 1.48
295 2.03 0.59
1653 2.03 1.02
2051 2.04 1.13
201 2.06 0.33
2094 2.06 0.84
2091 2.07 1.69
230 2.11 1.83
1351 2.12 1.65
2148 2.14 0.42
2106 2.16 0.59
1253 2.19 0.41
269 2.22 0.45
257 2.23 0.54
1647 2.25 0.85
2302 2.27 0.45
242 2.27 0.39
2079 2.31 0.44
265 2.32 1.19
1267 2.38 0.78
2077 2.41 1.51
286 2.45 0.54
1975 2.49 0.85
225 2.58 0.34
275 2.59 1.89
2138 2.65 0.88
2131 2.66 0.26
2065 2.7 0.77
2082 2.76 0.4
1282 2.87 0.96
263 2.98 0.51

Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.


Selection of best generic ID for ROM based devices like bq274xx


Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3142 bq27421-G1D: 4.4V LiCoO2 9.26
354 bq27411-G1C: 4.35V LiCoO2 11.92
128 bq27421-G1A: 4.2V LiCoO2 27.49
312 bq27421-G1B: 4.3V LiCoO2 36.78
Best generic ID 3142
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.


Device / Family #2
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 11.92
1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 13.76
1202 bq27621: (default) 4.2V LiCoO2 19.06
Best generic ID 354
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.


Device / Family #3
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 9.26
3230 bq27426: (default) 4.35V LiCoO2 11.96
1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 19.06
Best generic ID 3142
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.

请问一下这个 2487的化学ID如何找到,我已经把化学ID更新到最新版了------bqStudio Chemistry Updater (Rev. FF)