This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps23754简单应用电路,请大家帮忙检查

需要用TPS23754PW设计一个PD电源,按照TI手册及参考文档画了附件发原理图

设计输出为12V@2A,无辅助电源供电。

有几个疑问

1:负载最大功率为25W,分类class 4,CLS引脚接63.4欧姆电阻到VSS

      按照手册说明,class 4时最小负载功率为13W,如果此时负载不到13W,能否正常输出?

2:T2P引脚的功能不想使用,是否可以悬空处理,还是需要接上拉电阻到VC?

3:满载情况下发热量大的器件,除了两个电桥和变压器,还有哪些器件?

4:如果PSE端限制了每个端口最大输出功率为13W,PD端设计为class 4,PD端能否正常工作在最大13W的状态?

5:图中是否有错误或者不合理的地方?

TPS23754 POE SCH 0712.pdf