This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3060 remain capacity 计算方法

Other Parts Discussed in Thread: BQ3060

使用BQ3060时发现该Gas Gauge在低温使用时有些不正常,我们将充满的电池放在5℃的温箱中,放置1小时,然后使用5A放电,此时电池的剩余容量瞬间变成3%,然后持续放电直到保护,断开负载将电池放置20分钟让其恢复5℃后充电,此时电池的剩余容量一直都是0%直到TCA置位容量从0%突变至100%,请问如何设置才能避免该问题?

  • 请确认下在5'C条件下放电电流是多少C? 低温下电池内阻增大,过大的放电电流会导致电压急剧下降,gauge里都设定有EDV2,通常在3.3V~3.5V左右,电压被拉低到这个范围,电量会被强制拉到3%~7%,这种情况下最好减小放电电流。该链接工具可以调节EDV2电压http://www.ti.com/litv/zip/sluc042

  • 首先感谢您的回复,电池在5℃的情况下使用5C放电,但是放电一开始电池会被负载瞬间使用大概18C的速率放电1秒(我们使用的是磷酸铁锂电池)然后转至5C放电,所以您说的EDV2应该是该问题出现的原因,请问Luke,您说的EDV2是否是我们在GG文档中看到的Fixed EDV2?我们自己是否有办法可以修改EDV2的设定,比如delay time之类的寄存器?盼回复,谢谢!

  • 你使用的是磷酸铁锂电芯,再加上需要在低温下大倍率放电.建议你使用CEDV.LOG参数,计算CEDV的几个参数。