Other Parts Discussed in Thread: LM3478, LM5155, LM5121
需求:
1、输入电压为磷酸铁锂电池,单节并联,因此电压为2.5-3.5V;
2、输出希望为20-24V,1-2A,也就是功率可能高达20W-50W,非隔离。
问题:
1、有没有这样的芯片?按照功率计算电池的输出电流为6-20A,可能实现吗?
2、采用什么样的拓扑结构比较合适?
请专家指导解惑,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不需隔离,直接用外置MOS的升压芯片来做即可,只是如果输入最低2.5V, 而输出50W, 输入峰值电流接近30A,需要选择大功率的MOS, 建议在控制器之外增加MOS驱动器。
如果成本上允许,你可以多增加一级boost转换,用2个芯片分2次升压。
升压芯片,因为要加驱动芯片,所以选择较为简单的外置MOS升压芯片都是可以的。
谢谢专家,追问一下:
1、您指的MOS驱动的原因是不是芯片已经不能驱动大功率MOS,需要加一级驱动;
2、不考虑成本的话,2级升压的优势在哪儿呢?总体效率更低,也没有解决第1级大大电流问题,您觉得收益在哪儿?当然一些细节的考虑,比如1级升压的十几伏输出可以作为MOS的驱动电压,单级可能还是需要额外提供这个电压;
3、能不能请您推荐一下芯片,我看网站上得选择有LM3478/88系列、LM5155系列、LM5121/22系列,感觉都差不多,请您给优选一个吧,我们的应用场景是高温、高可靠性,因此还是有优选空间的。