This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM5085输出异常

Other Parts Discussed in Thread: LM5085

Hi:

   各位前辈,最近在使用LM5085做一个项目,需求是 8-36V输入 12V/5A输出,调式阶段有如下现象,当输入电压低于12V时  输出电压比输入电压低0.5V左右(加了二极管)而不是12V输出,  当输出大于等于12V输出为12V  电流正常  但是  1:输入电压大于18V左右 听到小小的吱吱声,输出正常 2:当输入电压大于20V以上输出电压正常 但是电流突然变大翻倍  电路板以及电源输入端二极管发烫 。  反馈电阻为  10K  1.18K 都是 1%,是什么原因导致呢?