This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21540 DT接到VCCI的逻辑是否可以实现



Dears,

如技术手册21页 9.3.2 Input and Output Logic Table中描述,将DT引脚直接连在VCCI上,INA和INB应该可以独立控制,输入都为高时,输出也应该都为高, 但实测中,INA和INB都为高时,两通道输出均为低,即真值表中DT接到VCCI的逻辑并不能实现。

在测试过程中关注了DT引脚电压,接RC时测量是0.8V左右,接VCCI时测量是4.98V左右。另外电路设计中DIS引脚对地接10K的电阻,测试过程中电阻一直存在。而且当输入INA和INB不同时为高时,输出逻辑与输入相同,理论上芯片是可以工作的。

烦请帮忙确定一下逻辑不能实现的原因在哪里,多谢!

Thanks!