This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

需要一个12V锂电池作为输入,输出7.2V的方案

如题

需要一个12V锂电池作为输入,输出7.2V的方案,此电源是给一款模拟放大器供电使用,想选用REG1117-ADJ,但是电阻太难搭配了。

哪位仁兄有可用的方案,请告知一下,谢谢

  • 你好,鉴于负载功率不大,有没有考虑LDO的方案?

    可以参考下用TPS7A4901,noise和SNR都很不错。

  • 感谢Liang sun的回复

    我现在在画板,使用的是REG1117-ADJ,他的输出公式为Vout=(R1+R2)/R1*1.25V

    R1和R2可以使用多个电阻串并联来实现非常规电阻的阻值,想问下有没有公式可以推导出R1和R2的组合,以输出7.2V。

    为了以防万一我在R2端加了一个可调的电阻,以实现动态的调整电阻。

    至于TPS7A4901,看了下手册,发现也是通过电阻搭配来输出想要的电压的,和1117类似。

  • 你好:

    按照上图,根据分压原理,假定Iin=0(忽略把馈引脚偏置电流的影响),可以推导出这个你写的Vout=(R1+R2)/R1*1.25V的公式,将Vout=7.2V代入,就可以推出R1和R2的一个关系。R2=4.76R1,你可以利用几个常规电阻串并联得到一个最接近的的比例关系。为减小误差,建议使用低容差的电阻。像117的手册第8页中建议使用1%容差的电阻。

    另外:建议避免使用小型可调电阻器,因为电阻器的成本高且长时间工作可靠性差。