| bq24780设置及读写状态值 1.bq24780设置 电池充电电流设置 寄存器 0x14 0x0200 电池充电电压设置 寄存器 0x15 0x1000 充电操作控制 寄存器 0x38 0x0304 报警状态控制 寄存器 0x3d 0x813b 2.bq24780状态读取 主电状态 寄存器 0x37 备电状态 寄存器 0x3a 通过上述设置后,电池充电电流只有几十mA,请问是那设置错了吗!原理图及PCB设计 按EVM板做的。可以实现主备电切换,及主备电状态的读取 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
• Charge is enabled through SMBus (REG0x12[0], default is 0, charge enabled)
• ILIM pin voltage is higher than 120 mV
• All ChargeCurrent(), ChargeVoltage() and InputCurrent() registers have valid value programmed
• ACOK is valid (see Device Power Up for details)
• ACFET and RBFET turn on and gate voltage is high enough (see System Power Selection for details)
• VSRN does not exceed BATOVP threshold
• IC temperature does not exceed TSHUT threshold
• Not in ACOC condition (see Device Protections Features for details)
这些条件没有不满足的,充电时,一开始有2A左右电流,然后,电流在20S内减少到几十mA