Other Parts Discussed in Thread: TPS61220
tps61220给1节3.6V锂电池升压,升到4.5V,当输出电流30mA时候,TPS61220电压输出被拉低到2.5v左右,看到手册上说可以输出200mA的电流,请问是什么原因导致电压被拉低呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61220
tps61220给1节3.6V锂电池升压,升到4.5V,当输出电流30mA时候,TPS61220电压输出被拉低到2.5v左右,看到手册上说可以输出200mA的电流,请问是什么原因导致电压被拉低呢?
数据手册里面标明的Minimum Switching Current 200 mA,并不是输出电流的大小,这是集成MOSFET的最小限流。Boost的IC的输出能力与输入电压,输出电压及集成的MOSFET的限流能力有关,需要通过计算才能得出最大的输出电流。可参考附件的公式3。但根据你的参数应该是能够输出30mA的。
另外当输出被拉低时输入电压是多少伏,使用什么样的电感,其饱和电流是否足够大?
Hi
请确认你选择的电感是适合于DC/DC的功率电感,饱和电流建议超过250mA.
另外注意输入电容layout靠近电感和Vin, 大小至少10uF,陶瓷电容。