This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895的OTG功能问题

Other Parts Discussed in Thread: BQ25895

During boost mode, the status register VBUS_STAT bits is set to 111, the VBUS output is 5V by default
(selectable via BOOSTV register bits).

手册上说明VBUS输出5V,但是在OTG模式下只有PMID输出了5V,VBUS输出0V,是不是手册写错了??????