使用TPS56121遇到的问题:
5V输入,1V输出,给板上的FPGA核心供电。
上电后输出正常,纹波40mV左右,但1~2分钟之后EN脚被拉低,输出端没有电压(此时FPGA没有配置,其他器件也都处于待机状态),调整反馈回路没有效果(有时一上电1V就没有输出)。
反馈环路计算使用TPS40KType III Loop Stability kVenable_sluc263c-071312.xls,按照datasheet中建议,Fco=50kHz,Phase Margin=60 degree。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS56121遇到的问题:
5V输入,1V输出,给板上的FPGA核心供电。
上电后输出正常,纹波40mV左右,但1~2分钟之后EN脚被拉低,输出端没有电压(此时FPGA没有配置,其他器件也都处于待机状态),调整反馈回路没有效果(有时一上电1V就没有输出)。
反馈环路计算使用TPS40KType III Loop Stability kVenable_sluc263c-071312.xls,按照datasheet中建议,Fco=50kHz,Phase Margin=60 degree。
1-2分钟后芯片是否有发烫的现象?没有输出电压跟补偿环路的关系不大,输出带多少安的负载?最好上传下原理图。ILIM接多少电阻?使用什么样的电感,是否电感饱和?并查看是什么原因导致EN被拉低。http://www.ti.com/lit/ug/slvu445b/slvu445b.pdf
输出为3V是空载,还是重载?分压电阻的选择可参考数据手册的公式16,如为更准确的设计可使用软件进行设计。
http://www.ti.com.cn/product/cn/tps56121 网页右边的WEBENCH进行设计。分压电阻使用4.53KΩ
没有存在压差为2V的说法,只要没有超过最大占空比:
数据手册里面有详细的设计实例,可先看一些基本的BUCK的电路设计。