5V输入,刚开始工作,三路分别输出1.2V 2.5V 3.3V正常工作,一分钟左右,第二路输出变为4V,测量RESET信号为5V,三路EN为2.5V,请问这是什么原因?MODE拉高为5V,采用的是自动上电模式,三路EN悬空。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5V输入,刚开始工作,三路分别输出1.2V 2.5V 3.3V正常工作,一分钟左右,第二路输出变为4V,测量RESET信号为5V,三路EN为2.5V,请问这是什么原因?MODE拉高为5V,采用的是自动上电模式,三路EN悬空。
一直是空载状态,FB在电压正常时是0.6V正常,一旦输出变化,FB也会发生变化,比如输出变为4.0V时,如果反馈脚为10K,10K,FB就会变为2.0V,稍后会把图贴出来,现在其实最奇怪的点在于,刚开始电路工作输出都是正常的,过一会输出至少有一路就会不正常。现在就想确认是否为电路问题还是芯片问题。