This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692输出电流无法达到设定值,LED微亮且抖动

RCS=0.05Ω,设定输出电流=3A,输出电压50v。

输入电压24v,电路稳定后,测得输出电压39v,测得PIN8/IMON引脚0.014v,输出电流仅20mA,LED微亮且轻微抖动。

以下是相关引脚的波形,希望专家帮忙分析,找出问题所在。

下图是电路稳定后PIN4/SS引脚的波形,是否正常?

\

下图是PIN10/PWM引脚的波形,频率200HZ,占空比50%。

下图是LED两端波形。

下图是PIN5/DM引脚波形。

下图是PIN12/PDRV引脚波形。

下图是PIN19/GATE引脚波形。