Other Parts Discussed in Thread: TPS60230
TPS60230 EVM 測到的quiescent current與SPEC中的不符,在Vin=4.2V, EN1=EN2=1, Iset=20uA 時測到5mA的Iq比SPEC 200uA大出許多
測試環境及條件都已照SPEC中的condition,請協助確認Iq過大原因。
謝謝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Vin=4.2V, EN1=EN2=1, Iset=20uA 这个规格应该是不完整的。 在有LED输出的情况下,Iset设定为20uA(Rset为30k), 此时LED的电流时20uA*260=5.2mA, 既然输出有这么大的电流,输入肯定是有较大电流的。
静态电流应该是在无负载情况下测试的,所以应该是在输出无LED的情况下测试(ILED=0), 请在增加这个条件后确认静态电流是否在规格200uA以内。
Hi
如果将EN1 和EN2 接GND, 测这个时候的shutdown电流将是多大?
Hi
另外请帮忙做一个实验,按照EVM板的电路,Vin=4.2V (EN1 = EN2 = 1,负载带有LED), Iset接一个6K的电阻,然后接一个600mV的电压输入,即采用模拟调光的方式使得输出电流为0(见datasheet第十二页模拟调光),测试此时的静态电流。
Datasheet对静态电流的描述不是很清楚,上述条件可以实现ILED=0,测试到的输入电流即4.2V时的静态电流。(因为我手头没有这块板子,上述实验麻烦了)
Dear Johnsin:
1.如果将EN1 和EN2 接GND, 测这个时候的shutdown电流将是多大?10uA
另外请帮忙做一个实验,按照EVM板的电路,Vin=4.2V (EN1 = EN2 = 1,负载带有LED), Iset接一个6K的电阻,然后接一个600mV的电压输入,即采用模拟调光的方式使得输出电流为0(见datasheet第十二页模拟调光),测试此时的静态电流。90uA
Datasheet对静态电流的描述不是很清楚,上述条件可以实现ILED=0,测试到的输入电流即4.2V时的静态电流。
所以x1-mode 就是指此模式(Iset接一个6K的电阻,然后接一个600mV的电压输入...)
TKS!!
Hi
是的,从目前的测试看No load quiescent current 是指ILED=0, 而非open-lamp(led)状态。
LED采用定电流设计,Open lamp(led) 会产生输出过压(5.5V),所以此时会引起较高的输入电流。