Other Parts Discussed in Thread: LM2731
您好,我最近在设计一款输入电压3V,输出电压7.5V,输出电流100mA的boost升压电路,采用了LM2731芯片进行设计,这是我按照官网模拟设计的参数图
我对这块板子进行测试,其中电源电压供电3V,电流设置限流60mA。然后带载进行测试,我的负载正常情况下工作电流3V/30mA左右,我对板子进行带载启动,无法启动,电流超限显红,电压被拖垮;我对限流值设置100mA则可以正常启动。
问题:
1.对于此款升压电路,我设计是否有问题,导致带载开机时,开机电流需要大于工作电流的两倍甚至更大?
2.该款boost升压电路,正常情况下带载开机是否电流会需求比较大?
3.该款boost升压电路,能否在较小电流的情况下带载启动?
4.其他boost升压电路,能否在较小电流的情况下带载启动?