想做一个4.5到5.5V输入,5V输入的电池管理方案,输出功率要大于3.5W,最好大于4W。电池为4.2到3V的,在4.2V到3V这个区间,都需要输出5V。不知道BQ24075是否合适。Datasheet上写的Selectable 100 mA and 500mA Maximum input Current应该怎么理解。我看输入电流最大能到1.5A呀。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.